The following diagram illustrates the response time for a dropout pulse from 90 % to 10 % of full-scale into a resistive load. Note that this waveform only illustrates the analog response. Programming response time, which is typically 25 ms, must be added to the analog response time.
The dropout (down-programming and up-programming) response time of the N8900-series is documented in the User’s Guide. Seehttp://literature.cdn.keysight.com/litweb/pdf/N8900-90901.pdf
Be aware that the down-programing time (falltime) with an open circuit can be as long as 30/40 seconds for the highest-rated current models, and as long as 10 seconds for all other models.
Applies to: N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8937APV, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A, N8957APV
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |